Mid-sized 12.1” display ready to rumble
Extending the 12.1” display size offering, Avnet Displays adds another bright addition to the SimplePlus Touch Display family — combining trusted performance with an even broader choice for our customers.
These days, very few displays use a parallel communication, and even then, it’s usually only for smaller screen sizes. For such RGB/TTL displays, the color information of every individual pixel is usually communicated over a parallel bus of 8 bits per color. This results in a 24-line width of the bus and, of course, this will also require a physically large connection cable. The TTL display uses higher voltage levels, compared to LVDS or MIPI displays. The communication is not as stable to external noise. Power consumption for TTL communication is higher, and the communication speed is slower.
All pretty good reasons to invent a better interface.
LVDS is a broad technical specification for signaling and uses differential signals of low voltage to send data. This can be seen in the connection cables used for LVDS signaling, where each wire is assigned to a different signal and the group is twisted to reduce the impact of surrounding electrical noise which would disturb the signal. You may see multiple twisted pairs within the display connection cable when it follows the LVDS specification.
Of course, we also see these twisted wires in a regular Ethernet cable, the type that typically connects a modem and a PC, but it doesn’t follow the LVDS specification. So, be mindful that twisted wires aren’t the automatic indicator of a display cable.
So, we know that both LVDS and MIPI displays follow the LVDS specification and have both differential signaling and twisted wire pairs, which naturally leads to the question: what does set them apart?
The key difference is in the protocol that defined communication over these twisted pairs (as well as some additional wires!). LVDS displays uses the Flat Panel Display Link protocol (FPD-Link), while MIPI displays use the MIPI Display Serial Interface protocol (MIPI DSI), which is a specification of the Mobile Industry Processor Interface (MIPI) Alliance.
When you stop using the acronym, the name is a bit of a giveaway. The MIPI DSI was designed as a cost-effective protocol for the displays in cellphones and other smart devices. So, using a system based on MIPI DSI can, theoretically, reduce the overall cost. But when viewed from a technical perspective, the story can be quite different. A MIPI display has significant layers of added complexity to consider and, overall, this results in a cost not that different to an LVDS display.
For example, MIPI has a TFT cell, it needs drivers, it needs intelligence to “translate” the serial data stream. It needs a backlight and housing. So, when even the components are largely the same, why is it often offered at lower price?
Assuming identical performance, ultimately it comes down to the fact that MIPI displays come from the consumer industry. Consider the sales figures of the world’s most popular smartphones and that will give you an indicator of the kinds of production volumes we are looking at. Vastly higher numbers than compared to, say, products in the industrial or medical world. Logically, higher volumes lead to more competitive component pricing and greater efforts to improve efficiency. So, just through sheer numbers, a high volume MIPI display will usually be cheaper when compared to an LVDS display.

Extending the 12.1” display size offering, Avnet Displays adds another bright addition to the SimplePlus Touch Display family — combining trusted performance with an even broader choice for our customers.

Technologies tend to come full circle, but in this case we mean literally – combining an advanced rotary encoder (and encoder shell) with a 1.28-inch circular TFT display for a single, compact control solution. Users can navigate with precision by simply turning or pressing the knob, while the integrated screen displays menus, status updates or graphics right at the point of interaction.
Additionally, as many microprocessors and microcontrollers can drive MIPI displays directly, no display driving board is required to translate the data stream of the processor into the FPD-Link data stream. The intelligence of the application also controls the display directly. This too eliminates components and reduces the overall system price.
However positive and appealing this may see, we do have to address the ‘elephant in the room’. Yes, we benefit from a volume cost saving with MIPI – but this cost saving comes from the same place as MIPI’s key risk: that such displays are aimed at the consumer market. This means that many of the products are not designed with the same longevity in mind as an industrial or medical application (which require many years of support). They are not as sturdy when compared to industrial displays and their integration may be more difficult (e.g., screw-in mounting is not supported). Certainly, we would never advise selecting such a display for use in the medical or industrial world.
This said, they offer excellent benefits for a whole range of product groups – as long as you have a solutions partner who has expertise in ‘driving’ MIPI. Because no two MIPI displays are alike, there are some physical, electrical and communication related adjustment required, and our experts and engineers know them all. Having the right expert at hand who selects you MIPI displays with longevity in mind, who properly considers the levels of robustness required and has the ability to establish proper display driving is essential. And can help you to bring all the benefits of MIPI DSI displays into the prosumer or even the industrial world.
|
|
Frank Ploenissen - Marketing Manager Display Integration, Avnet at Avnet After getting his diploma in electrical engineering, Frank entered the world of display solution and distribution in the year 2000, holding product responsibility for several display and touch lines. Starting 2007 he worked as a sales and marketing manager for a design and manufacturing company of CCFL and LED backlight drivers, and afterwards established the German branch for a Austrian display and solution provider. In 2013, Frank joined former MSC which in turn was bought by Avnet. In his current role as Marketing Manager Display Integration, Frank and his team supports the Avnet team and their customers concerning the integration of display products into customer applications and steers and extends the product lines of SimplePlus and MipiPlus display solutions.Read More |
Our Avnet Displays come in a range of form-factors and our display-experts are on hand to guide you in the creation of display or touch solutions that meet your requirements. Find out how Avnet Displays can propel your product innovation and get in touch today.
Let us know about your product or your challenge and our team will get in touch to discuss how we can help.
Your privacy is important to us.
We use cookies to enhance your experience when visiting our websites: performance cookies show us how you use this website, functional cookies remember your preferences and targeting cookies help us to share content relevant to you. Select "Accept all" for giving your consent to all cookies, select "Cookie settings" for managing the different cookies or select "Reject all" for using only strictly necessary cookies. You can change your cookie settings at any time by clicking on the cookie settings link on the website.