Widen your view – with the MipiPlus 6.8”

By Frank Ploenissen | 28 February 2024

The keen-eyed among you will have noticed that every couple of months we share news of an addition to our MipiPlus range. Well, it’s a product family that just keeps growing. Why? Because you want it to. And today we’re welcoming the MipiPlus 6.8”.

A wide format (17.27 cm) MIPI DSI display, the MipiPlus 6.8” has a higher speed and greater functionality when compared to the standard RGB or LVDS interfaces.

And it’s even more compact than the existing MipiPlus 7” display, while still offering a very good pixel resolution, with a wide viewing angle that means it can be used in both portrait and landscape mode.

Coupled with high brightness and industrial temperature range, it’s ideal for use outdoors in small size applications, such as door intercoms, secondary displays for vending machines, handheld video appliances and plenty more besides.

It has touch functionality integrated in the module, and the 1.8 mm protective front glass with neutral black border print gives the display an attractive and sleek design. MipiPlus 6.8” can also be directly connected to many modern microcontrollers and microprocessors.

Mipiplus
Resolution 480x1280 pixel
Outline 100.0 x 200.0 x 9.55 mm
Viewing Angle 160v/160h
Brightness 1000 nits TFT brightness (w/o Touch+Glass)
Contrast 1500:1 contrast
Temperature -20° C to 70° C
Product Code: XEA-068A01-DI9509-G020

Of course, all Avnet Displays MipiPlus products are part of our established and popular SimplePlus™ program, which creates a reliable production process, based on tested and proven concepts, for your volume projects. SimplePlus™ offers rapid delivery of single samples, customization options and other design adjustments, and can significantly decrease overall material costs and development time while boosting production efficiency. We also provide support drivers for Linux for easy implementation into the software stack.

Other articles

Feel the noise with multimodal HMI combining haptic and sound

When we touch, we like to feel. When we press our fingers against something, our brains have been conditioned to expect some kind of feedback. So, if we tap a flat screen and get nothing in return – no physical or audio response – it doesn’t feel right. Which is why we are introducing new Human-Machine Interface (HMI) solutions that combine Piezo Haptic Technology with Sound Actuators (Exciters).

Read More »

About Author

Frank Ploenissen - Marketing Manager Display Integration, Avnet at Avnet

After getting his diploma in electrical engineering, Frank entered the world of display solution and distribution in the year 2000, holding product responsibility for several display and touch lines. Starting 2007 he worked as a sales and marketing manager for a design and manufacturing company of CCFL and LED backlight drivers, and afterwards established the German branch for a Austrian display and solution provider. In 2013, Frank joined former MSC which in turn was bought by Avnet.
In his current role as Marketing Manager Display Integration, Frank and his team supports the Avnet team and their customers concerning the integration of display products into customer applications and steers and extends the product lines of SimplePlus and MipiPlus display solutions.
Read More

Our Avnet Displays come in a range of form-factors and our display-experts are on hand to guide you in the creation of display or touch solutions that meet your requirements. Find out how Avnet Displays can propel your product innovation and get in touch today.