Mid-sized 12.1” display ready to rumble
Extending the 12.1” display size offering, Avnet Displays adds another bright addition to the SimplePlus Touch Display family — combining trusted performance with an even broader choice for our customers.
Electronic paper (also known as e-ink, electrophoretic display, or electronic ink) is a kind of electronic display that mimics the appearance of ink on paper. An electronic paper display reflects ambient light like paper, unlike conventional flat panel displays that emit light.
Lightweight and slim, ePaper displays offer high-resolution and no glare visibility, allowing users to view text and pictures at any angle, giving them paper-like readability – even outdoors and in bright sunlight, without the need for a backlight. This makes it the perfect choice for both indoor and outdoor displays, such as retail shelf labels, interactive museum signs, traffic signs, notice boards and passenger information boards.
But outside of usability, they are predominantly known for their durability, reliability, high data storage and low power consumption. It can hold static text and images for an indefinite time without the use of electricity and will continue to display content even in a power outage. This is because it doesn’t require power to display an image, only to change the content. Equally, the response time of ePaper displays is slower when switching between screens. This too makes them more suited to static image displays.
Their displays will use approximately 3 mA for 2 seconds each time it updates its contents, giving full use of 36 mA or 0.012 mAh per day. Therefore, the display consumes only 0.008% of the power that a same-sized TFT LCD would require in a day and because there is no heat source, there is equally no heat dissipation. With the global focus on energy conservation, ePaper has a major advantage over traditional LCD screens and, as a result, the market demand is increasing.
To make the ePaper smart, so that it can be used in ebooks, wearable electronics and others, it is necessary to add a PCAP.
The main challenge in optical bonding EPD and a PCAP is the very thin glass substrate. Excessive or uneven pressure applied during the bonding process can cause the glass to break. And the traditional liquid bonding may result in adhesive overflow, and the curing shrinkage of the adhesive can lead to mura issues.
To tackle these two pain points, we use solid OCA (silicone-based) for the optical bonding procedure. The pressure and debubbling pressure used in vacuum bonding are low, which, combined with our self-developed bonding fixtures, avoids excessive and uneven pressure. This also reduces the occurrence of stress-related mura. To increase weather-resistance, we can incorporate anti-UV designs into the structure to prevent the LCD yellowing or cracking.
Smart ePaper displays are well suited to plenty of Smart Cities applications, as well as Public Information Displays, digital signage, electronic billboards and transportation vehicles, among others.

Extending the 12.1” display size offering, Avnet Displays adds another bright addition to the SimplePlus Touch Display family — combining trusted performance with an even broader choice for our customers.

Technologies tend to come full circle, but in this case we mean literally – combining an advanced rotary encoder (and encoder shell) with a 1.28-inch circular TFT display for a single, compact control solution. Users can navigate with precision by simply turning or pressing the knob, while the integrated screen displays menus, status updates or graphics right at the point of interaction.
We offer a variety of value-added features tailored to different applications, as well as customized integration services:
Our PCAP technology stable against noise, water, humidity, thanks to the mutual differential technology and HW FFT to find the best low noise frequency.
|
|
Stefano Rosato - Director, Technical Touch Technology at Avnet Stefano Rosato is director of technical touch technology in the Display Solutions team at Avnet. Stefano helps customers solve touch challenges and supports customers through the whole design-in phase for touchscreen integration. With deep knowledge about PCAP technology, along with its design-in rules, tuning and pattern designs, Stefano is a leading expert in the touchscreen industry.Read More |
Our Avnet Displays come in a range of form-factors and our display-experts are on hand to guide you in the creation of display or touch solutions that meet your requirements. Find out how Avnet Displays can propel your product innovation and get in touch today.
Let us know about your product or your challenge and our team will get in touch to discuss how we can help.
Your privacy is important to us.
We use cookies to enhance your experience when visiting our websites: performance cookies show us how you use this website, functional cookies remember your preferences and targeting cookies help us to share content relevant to you. Select "Accept all" for giving your consent to all cookies, select "Cookie settings" for managing the different cookies or select "Reject all" for using only strictly necessary cookies. You can change your cookie settings at any time by clicking on the cookie settings link on the website.