A monitor with a three-in-one cable? Pure simplicity.

By Stefano Rosato | 5 December 2024

There are two words guaranteed to make us sigh loudly: cable management. Now, don’t misunderstand us, we know the unique satisfaction of well managed cables, but that feeling is entirely derived from the knowledge that they often need a lot of wrangling.

Take monitors, for example. There are plenty of situations where having multiple cables attached to a monitor can be obstructive and problematic. On medical devices, where additional cables mean more cleaning to maintain high levels of hygiene. Or kiosks and Point of Sale systems, where a streamlined look and zero public obstruction is essential.

See? Cables matter. So much that our customers have been asking us for help.

And, of course, our design experts were all too happy to spring into action, doing what they do best, and have solved the cable conundrum with a new USB-C Monitor Series that is a single cable dream. In your traditional monitor setups, you would expect to have separate cables for power, touch functionality and a video data cable, such as an HDMI.

Our new USB-C Monitor Series needs only a single cable to handle all three.

The range covers display sizes from 10.1” to 21.5”, sizes we know to be popular in commercial, medical and industrial environments. And, because our team think of everything, the monitors also support VCP (Virtual Control Panel) commands over USB-C, so you can monitor and adjust brightness, contrast and color. Commands can be sent directly from the host device without needing physical buttons or complex control setups, allowing for easier configuration and remote adjustments.

Plus, the maximum cable length of three meters means that the monitor can easily be positioned further away from the host system, while maintaining signal integrity. This is ideal for industrial and commercial setups where the monitor and controlling system may not be directly next to each other.

It all comes down to one thing: simplification. Our new USB-C Monitor Series cuts through the complexity of traditional setups with a single cable, making these monitors perfect for today’s demanding industrial and commercial environments.

Avnet USB-C Monitors: Technical Features
High Brightness: 1000 cd/m² brightness makes them suitable for both indoor and outdoor use, even in environments with strong ambient light.
Durable: These displays can withstand harsh environments, making them perfect for industrial or rugged applications.
Capacitive Touch Technology: 10-point capacitive touch supports both finger and capacitive stylus interactions, this means precise and responsive user input across multiple applications.
OSD: On Screen Display Controls for quick adjustments, while the main controls can still be driven via USB-C commands for remote access.
Energy Efficient: Suitable for continuous operation in power-sensitive environments.

Other articles

Turning control into clarity: our latest encoder with TFT

Technologies tend to come full circle, but in this case we mean literally – combining an advanced rotary encoder (and encoder shell) with a 1.28-inch circular TFT display for a single, compact control solution. Users can navigate with precision by simply turning or pressing the knob, while the integrated screen displays menus, status updates or graphics right at the point of interaction.

Read More »

About Author

Stefano Rosato - Director, Technical Touch Technology at Avnet

Stefano Rosato is director of technical touch technology in the Display Solutions team at Avnet. Stefano helps customers solve touch challenges and supports customers through the whole design-in phase for touchscreen integration. With deep knowledge about PCAP technology, along with its design-in rules, tuning and pattern designs, Stefano is a leading expert in the touchscreen industry.Read More

Our Avnet Displays come in a range of form-factors and our display-experts are on hand to guide you in the creation of display or touch solutions that meet your requirements. Find out how Avnet Displays can propel your product innovation and get in touch today.