Tinnitus Treatment Device
This crowdfunding project resulted in a great product for effective tinnitus treatment.
This crowdfunding project resulted in a great product for effective tinnitus treatment.
Due to our good customer relationship, we got a request for their new high-brightness
We had 2 years of consistent approach and lobbying to gain the customer’s confidence and convince them to redesign
Thanks to strong relationship with our supplier, we were able to offer very fast and precise support
Avnet won a new project with one of our existing customers. They were interested in an ~1 inch MIP
The customer was informed about the products from our sales long before this project started
This is our second project win with this customer who initially wanted to cancel a running contract of a different product
The customer searched for a customized monitor with just 500 pcs/year. Avnet was able
Our sales team has built a very good relationship with a customer in Spain, who provides mobility solutions
Our sales team has built a very good relationship with a customer in Spain, who provides mobility solutions
The end-customer asked their EMS for a new product. Due to our good contact
with them
Our well-known customer used a 3rd party to upgrade their 7” display to 1000 nits
Our customer had a well running series with the previous display from us and asked for a fitting solution for a new
Our customer asked for the second source with 100% compatibility of their current series
Our customer asked for the second source with 100% compatibility of their current series
The customer wanted to replace their current vendor from Korea with a given target
Our customer needed an impact-resistant display with PCAP for outdoor use in rain and snow at a budgetary price
The customer had issues with current supplier and requested a reliable supplier with stable longevity
Thanks to our good relationship with the customer, we were able to offer for a tender. We negotiated the
Through effective communication between our supplier, customer and Avnet, we were able to build a strong
To win this project with an off-the-shelf TFT, we visited the customer together with the manufacturer and negotiated
One of the suppliers supported the project with high flexibility for customization and could hit the tight timeframe
The customer wanted UHD or FHD and we recommended FHD from one of the suppliers
For the low power requirement, Avnet proposed a MIP display with supplementary lighting to ensure readability in low-light conditions.
Our sales team maintained a good relationship with the design house, which preferred
A new display win, and I definitely want a sample! This is a touchscreen display
For this tender the end-customer asked for 12.1” size what was not in the standard portfolio of our
At the start, we had to overcome EMC issues, caused from the connection of the metal oven connected
Due to good relationship to supplier and customer, Avnet built a growing display business with the customer
We do many design-in´s in the marine segment, but this time it was exceptional, because the demand was for
4.3″ LCD module was designed to meet and exceed industry standards in pump control and monitoring. Tailored precisely
The system controller is coordinating data to and from the individual refrigeration and HVAC controllers
Thanks to our strong customer relationships, we received requirements for all new product series. We delivered both
Our customer wanted direct manufacturer contact and also the complete product from one manufacturer, so
Through consistent communication and comprehensive technical support, we delivered a 100% compatible
The photovoltaic market is experiencing rapid growth. Solar panels generate DC power, but it’s solar inverters that transform
For this challenging application customer needed a 7″ PCAP panel mount HMI to work in harsh environments
This project’s challenges involved providing various bonding, taping, FPC design options, and quality
Our team successfully developed a cutting-edge display for a handheld eye treatment device, overcoming challenges
This huge project is based on a really long relationship. The customer was looking for a complete
This project, lead by our US team, presented challenges like PCAP integration, the need for a fast sample
We had several challenges for the Li-ion tool chargers project, including display parameter requirements, a high degree of customization, and a critical need for a fast delivery
Out touch team has done a great work for this project tuning touch to an outstanding performance
The handheld sonar enables rescuers to quickly identify potential victims within seconds of entering
The customer´s main needs focused on achieving improved optical performance and a more competitive price than the current design
The combination of specially coated coverglass, high surface hardness and optical bonding offers
The customer needed to update their product design for the next version of their range of different size chargers for residential buildings
Our customer wanted to have a larger display for their current portable device. Interface, pinning
It takes very long to get all metric certifications in each country, so that a very long product lifecycle
The customer asked for a sunlight and night readable display with better optical performance than the running one
The customer faced intense time pressure and had a big requirement catalogue. To address this
The customer specializes in high-end residential chargers for multi-car households and large garages
The customer´s main need was a display-touch-coverglass stack fulfilling IK9, outdoor readability
There were high requirements towards quality and reliability. The customer needed a very long product life
We visited the customer to investigate the mechanical design of the product and the specific frame mounting requirements
The customer required a display for a commercial, heavy duty hydrogen filling station for heavy goods vehicles
The customer needed a display to fit into the existing mechanics.
Apart from that, the most important requirements were sunlight readability, shock & vibration resistance, UV resistance and very low power consumption.
The customer had EMI issues with his current series and wanted to improve the display. They needed a robust outdoor readable display with wide temperature range within a price target.
The customer offers retrofittable reversing camera systems for different kinds of vehicles.
The requirement catalogue for optical performance was big and additionally they needed a wide temperature range and a defined FPC as well as good scratch resistance.
The customer developed a solar operated car and needed an infotainment display that fitted into their electrics and mechanics
The customer required a rugged outdoor fast charging application. They needed to reach mass production
A complete solution with embedded board was required and so we offered a customized display-touch unit with a customized SMARC module.
Your privacy is important to us.
We use cookies to enhance your experience when visiting our websites: performance cookies show us how you use this website, functional cookies remember your preferences and targeting cookies help us to share content relevant to you. Select "Accept all" for giving your consent to all cookies, select "Cookie settings" for managing the different cookies or select "Reject all" for using only strictly necessary cookies. You can change your cookie settings at any time by clicking on the cookie settings link on the website.